AXIS#.IL.CMD
Description
AXIS#.IL.CMD displays the q-component current command value of the current loop after any limitation (such as a parameter setting or I2t calculation).
AXIS#.IL.CMD is limited also by motor peak current, AXIS#.IL.LIMITN and AXIS#.IL.LIMITP .
Versions
Action | Version | Notes |
---|---|---|
Implemented | 02-00-00-000 |
General Information
Type |
Read Only |
Units |
Arms |
Range |
± Drive peak current (IPEAK) |
Default Value |
N/A |
Data Type |
Float |
See Also |
|
Stored in Non-Volatile Memory |
No |
Variants Supported
All variants are supported
Related Topics
Fieldbus Information
Name |
ID |
Hex |
Data Type |
Access |
Units |
---|---|---|---|---|---|
AXIS1.IL.CMD |
5801 |
16A9 |
Signed32 |
Read Only |
- |
AXIS2.IL.CMD |
71337 |
116A |
Signed32 |
Read Only |
- |
Parameter |
PNU |
Data Type |
Access |
Units |
---|---|---|---|---|
AXIS#.IL.CMD |
5801 |
Float |
Read Only |
- |